电池组放电过流保护后,电池电压可能已经低于MAX17055的供电电压,而由于MAX17055没有非易失寄存器,所以数据会丢失。针对这个问题,可以将MAX17055放在电池与保护电路之间,这样即使保护电路侧没有输出了,电池仍然可以给MAX17055供电。如果在用MAX17055评估板软件配置MAX17055,则可以将软件Configure页面的右上角POR后的Automatically Restore IC Settings after Reset 选中,这样MAX17055重新后评估板软件就会自动将上次对于电池参数的配置重新写入MAX17055.