在使用MAX17205时读取的温度值不正确,因此,想通过读取nPackCfg寄存器来验证I2C通讯的正确性,期望读取到默认的0xa02,而实际得到的是0x05,可能是没有正确理解内部寄存器的地址是如何映射的,能详细介绍一下这方面的内容吗?
问答
文档
成员
标签
Cancel
文档
+
AD
+
DS
+
General
-
MAX1x
+
MAX14690AEWX+: FAQ
MAX14745: FAQ
MAX14745AEWX+: FAQ
+
MAX14745AEWX+T: FAQ
MAX14921: FAQ
+
MAX14921ECS+T: FAQ
+
MAX17043: FAQ
+
MAX17047G+: FAQ
+
MAX17048: FAQ
+
MAX17049G+: FAQ
+
MAX17055AEWL+: FAQ
+
MAX17058: FAQ
+
MAX17201/MAX17205: FAQ
+
MAX17201G+T: FAQ
MAX17205: FAQ
-
MAX17205G+: FAQ
4节串联的锂电池接到MAX17205评估板后,评估板软件显示有错误,原因是什么?
MAX17201/17205的I2C从机地址是什么?
max17205 在测量电流为负时,如何根据测量的数字信号来计算电流值。比如Current值为0xF163 即 61795,怎么算出来是-584.531?
MAX17205内部的过流比较器带有一个可编程的去抖延迟设置,请问该比较器具体是如何工作的?
MAX17205在设置电池容量是直接将数据转换成16进制数据写入nDesignCap Register(1B3h)吗?
MAX17205如何检测电池的温度,要配置哪些寄存器,读哪些寄存器?
MAX17205应该设置哪些寄存器才能读到正确的剩余电量?
MAX17205是否支持镍隔、镍氢电池等?
max17205的i2c访问地址应该是0001011x还是0010110x ?
使用MAX17205时,软件读出的电压、电流、温度数据都正确,但RepSOC始终为1.0%,为什么?
在使用MAX17205时读取的温度值不正确,因此,想通过读取nPackCfg寄存器来验证I2C通讯的正确性,期望读取到默认的0xa02,而实际得到的是0x05,可能是没有正确理解内部寄存器的地址是如何映射的,能详细介绍一下这方面的内容吗?
在使用MAX17205测量电量时,读取电池电压和器件名称正确,但是读取的电流值始终为0,请问是什么原因?
如何使用MAX17205获取电池电量?
将nLearncfg 寄存器设置为 0x2672 后MAX17205G充电电量不准,什么原因?
读取MAX17205的哪个寄存器,来获取电池是充电还是放电状态。
针对大容量、多节串联的锂离子电池,有没有比较好的电量计方案?
+
MAX17205G+T: FAQ
+
MAX17211G+: FAQ
MAX17260: FAQ
+
MAX17260BEWL+: FAQ
+
MAX17261METD+: FAQ
+
MAX17261XEVKIT: FAQ
+
MAX17262 EVALUATIO: FAQ
+
MAX17262MEWL+: FAQ
+
MAX17263: FAQ
+
MAX1737: FAQ
MAX17435ETG+: FAQ
+
MAX17435ETG+T: FAQ
+
MAX17435EVKIT+: FAQ
MAX17572: FAQ
+
MAX17572ATC+: FAQ
+
MAX17830GUN/V+_T1: FAQ
MAX17841BGUE/V+: FAQ
+
MAX17841BGUE/V+T: FAQ
MAX17843ACB/V+: FAQ
+
MAX17843ACB/V+_T1: FAQ
+
MAX1873TEEE+: FAQ
+
MAX2x
+
MAX6x
+
MAX7x
+
MAX8x
在使用MAX17205时读取的温度值不正确,因此,想通过读取nPackCfg寄存器来验证I2C通讯的正确性,期望读取到默认的0xa02,而实际得到的是0x05,可能是没有正确理解内部寄存器的地址是如何映射的,能详细介绍一下这方面的内容吗?
关于内部寄存器地址分配的介绍在数据手册第99页的Table27中。
如果寄存器地址小于0xFF,器件的从地址为0x6C.
如果寄存器的地址大于0xFF而小于0x180,从地址为0x16,寄存器地址0x00--0x7F对应于0x100-0x17F寄存器。
如果寄存器的地址大于0x17F,从地址为0x16,0x80--0xFF对应于0x180--0x1FF寄存器。
Tags:
能源存储系统(ESS)和电池管理系统(BMS)
000094181
MAX17205
Share
History
Cancel
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.