Post Go back to editing

接近满电的电池,放置一段时间后,mcu重新配置一次电量计配置参数,获取的soc为25%左右

Category: Software
Product Number: MAX17261

我之前测试过,如果只在电量计掉电前配置一次电量计,在几次充放电后,满电后电量计的soc只有80%左右,为了不出现这个问题,每次系统上电时,都会重新配置一次电量计。总共几十台设备,出现了2台设备获取的soc为25%左右,插入适配器冲一会电后,电量会达到95%,mcu断电静置一段时间后重新配置一次电量计,soc又会变为25%左右

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.