同样的程序,我用电脑typec给6804供电可以收到数据.但是从电池侧转压(我已测量确实为5V)就不可以了.我使用的是转压芯片,因为我在用三极管测试的时候发现电压只有3V.希望工程师可以解决我的问题
LTC6804-1
Not Recommended for New Designs
The LTC6804 is a 3rd generation multicell battery stack monitor that measures up to 12 series connected battery cells with a total measurement error of...
Datasheet
LTC6804-1 on Analog.com
同样的程序,我用电脑typec给6804供电可以收到数据.但是从电池侧转压(我已测量确实为5V)就不可以了.我使用的是转压芯片,因为我在用三极管测试的时候发现电压只有3V.希望工程师可以解决我的问题
您好,方便给出原理图吗?但是从电池侧转压(我已测量确实为5V)就不可以了.我使用的是转压芯片,因为我在用三极管测试的时候发现电压只有3V.很抱歉,因为我不了解您的实际测试条件和电路,加上描述有点模糊,您这里说的5V和3V应该都是Vreg的供电吧?但什么条件下有5V,请您再说清楚点,还有就是三极管如果供电只有3V应该是异常的,不能工作的。您说用电脑给6804供电,指的是电脑typec直接5V给Vreg供电?
如果您用电池包本身取电,Vreg只有3V,可能是您再三极管在集电极上的压降太大了,导致Vc电压也很低,三极管可能饱和了。您可以测下您三极管Vc上的电压。

感谢您的回复,我的问题已经自己解决了.
工程师您好,我遇到了新的问题,我使用了LTC6811官方代码中的断线检测函数,但是不能准确识别断线.请问该如何解决这个问题