我按照数据手册上面的要求,写入COMM寄存器数据(0x721),然后启动IIC传输(0x723),而后延时72个时钟周期,并且保持CS片选高,但是GPIO4和5端始终没有信号输出。
并且验证过COMM寄存器里确实被写入了数据,GPIO寄存器查询结果也为1,端口上拉后电压4.5V。这个问题困扰了很久,求解答。
LTC6813-1
Production
The LTC6813-1 is a multicell battery stack monitor that measures up to 18 series connected battery cells with a total measurement error of less than 2...
Datasheet
LTC6813-1 on Analog.com
我按照数据手册上面的要求,写入COMM寄存器数据(0x721),然后启动IIC传输(0x723),而后延时72个时钟周期,并且保持CS片选高,但是GPIO4和5端始终没有信号输出。
并且验证过COMM寄存器里确实被写入了数据,GPIO寄存器查询结果也为1,端口上拉后电压4.5V。这个问题困扰了很久,求解答。
片选拉高?片选应该是拉低,这个波形是正常的波形,你按如下波形的时序要求去复现即可。
确实是因为stcomm指令后的cs被拉高了一下,已解决,谢谢