您好,我们现在需要调试384串电池读取数据,使用菊花链的方式串32个6812用来读取,请问有哪些需要注意吗? 6812最多可以串多少节电池,时序读取的等待时间和读取的速率多少比较合适?
LTC6812-1
Production
The LTC6812-1 is a multicell battery stack monitor that measures up to 15 series connected battery cells with a total measurement error of less than 2...
Datasheet
LTC6812-1 on Analog.com
您好,我们现在需要调试384串电池读取数据,使用菊花链的方式串32个6812用来读取,请问有哪些需要注意吗? 6812最多可以串多少节电池,时序读取的等待时间和读取的速率多少比较合适?
ltc6812最多可以监测15节串接电池,读写时候注意measure core 的看门狗休眠时间2s.和isospicore 的tidle tready和twake up这些时间规范。读取速率最高不超过1M合适。adc采集指令发送后,建议用pladc指令来精确定位数据回读时间,而不要用简单的延时。当然,我这边无法覆盖掉时序上要注意的所有细节,更多细节你可以查看手册,并在遇到问题后可以来这边提问。
我看规格书上面,通过6820转换的2线isospi可以分别在6812的两端读取,但是现在我在测试中发现只能从IMB&IPB端可以读取到数据,请教下硬件连接上面有什么区别吗
硬件连接上没有区别。从partA唤醒就从partA读,从partB唤醒就从partB读,你现在电路中的isospi通信是设计成什么样的。