Post Go back to editing

关于LT8301隔离电源设计问题

Category: Hardware
Product Number: LTC8301

关于LT8301的电源设计,有如下疑问:

1、根据LT8301规格书第一页的典型应用拓扑,是不是可以理解为在输入电压2.7V~36V,LT8301都可以稳定输出5V。

2、但根据规格书提供的参数计算来看,与第一页拓扑中的变压器参数对应不上,与第19页的典型应用拓扑中的参数也无法对应。典型应用拓扑中的参数是如何确定的。

3、当前我需要设计一款隔离DC电源,输入4V~35V,输出5V 0.2A。是否有合适的方案推荐,以及LT8301的计算工具可以辅助我进行计算及仿真。

以上,期待技术指点,谢谢

Parents
  • 以上,第一页和第19页是完全对得上的,不一样的是变压器的原副边比例,

    LTspice就可以很方便的进行LT8301的仿真和计算,务必留意输入不同时,负载的电流输出能力,确实是输入2.7-36V负载都能保证稳定不变的电压,前提负载电流在规格之内,仿真时候呢,先建议将负载阻值调大点,有利于你观察,之后可以根据你负载的实际大小,设计输入电压值范围。

Reply
  • 以上,第一页和第19页是完全对得上的,不一样的是变压器的原副边比例,

    LTspice就可以很方便的进行LT8301的仿真和计算,务必留意输入不同时,负载的电流输出能力,确实是输入2.7-36V负载都能保证稳定不变的电压,前提负载电流在规格之内,仿真时候呢,先建议将负载阻值调大点,有利于你观察,之后可以根据你负载的实际大小,设计输入电压值范围。

Children
No Data