Dear
How to assigned ADBMSA18181 slave address while on the daisy-chain state ?thanks in advance
ADBMS1818
Recommended for New Designs
The ADBMS18181 is a multicell battery stack monitor that measures up to 18 series connected battery cells with a total measurement error of less than 3...
Datasheet
ADBMS1818 on Analog.com
Dear
How to assigned ADBMSA18181 slave address while on the daisy-chain state ?thanks in advance
ADBMS1818在菊花链中的通信方式采用的是无地址的通信方式,采用的是无寻址的通信,所以一般一个指令下去,所有芯片执行的都是同一个指令。详细的1818通信方式,可以参考ltc6820芯片手册的阅读,看完应该能对1818的isospi通信方式有个很好的理解。
ADBMS1818在菊花链中的通信方式采用的是无地址的通信方式,采用的是无寻址的通信,所以一般一个指令下去,所有芯片执行的都是同一个指令。详细的1818通信方式,可以参考ltc6820芯片手册的阅读,看完应该能对1818的isospi通信方式有个很好的理解。
谢谢你的回复,根据1818这样的通信方式,我客户研发那边还有一个疑问:
多级的菊花链连接下,读取电压或者温度发送一条指令后,从机按照顺序返回data可以理解,但是如果需要单独控制多从机下指定的从机通信情况,该如何操作呢?
举例:1个主机,10个从机,现在需要单独控制第5个从机的电压均衡策略,别的从机不操作。如果主机下发均衡指令,所有从机都回复均衡操作,这似乎不太合理。实际指令需求只是需要从机5响应。
所以针对主机如何选定特定从机5进行通信问题改如何操作呢?
谢谢
discharge动作,不同于广播指令,是需要写每片是configA寄存器触发的,所以,就是仍然可以做到均衡的定点可控。
其实虽然是无寻址的操作,但是功能用起来总能找到对应的实现方法和指令,客户可以具体问题具体分析,解决不了可以过来提问。