Post Go back to editing

LT8490 LDO33 voltage is wrong,LT8490 not work

Category: Hardware
Product Number: LT8490

According to the 27.4V lithium battery charging circuit in the LT8490 manual, the voltage of the LDO33 is not 3.3V after charging with the solar cell simulator。

LDO  2.394V

ADD  2.394V

VDD  2.394V

SWENO: 0V

SWEN: 0V

How is the voltage of LDO33 affected? The other parts of the circuit are designed by examples, and the resistance values are configured correctly. We cannot find why the voltage of LDO33 is not 3.3V.

Thanks

Thread Notes