Post Go back to editing

COM port not recognized in connection

When using CN-0510 development board, an external disk pops up after inserting USB, but COM cannot be found in Analog Devices SensorPal. How can I solve this situation? thank you

Thread Notes

Moved from 论坛社群活动 to 能源存储系统(ESS)和电池管理系统(BMS) on Monday, November 13, 2023 2:09:55 AM by Admin_ADI
Moved from 论坛社群活动 to 能源存储系统(ESS)和电池管理系统(BMS) on Monday, November 13, 2023 2:09:55 AM by Admin_ADI

  • 是第一次遇到这个问题吗?还是之前使用正常,现在突然不正常了的?

  • 之前还是可以正常使用的,出现这个问题一直没有办法恢复。尝试进入维护驱动模式更新接口文件,SensorPal可以识别得到COM口但仍无法连接成功,请问这是什么原因引起的呢?非常感谢。

    It can still be used normally before, and there is no way to recover this problem. When I tried to enter the maintenance drive mode to update the interface file, SensorPal could identify the COM port but still failed to connect to it. May I ask what caused this? Thank you very much.

  • 重装软件问题能得到解决不,目前不知道这种错误的来源,可能是驱动和操作系统哪里冲突了。

  • 你好,这个问题没得到解决,重新购买了一块3029电路板。

    想请教你一个问题:现在需要使用CN-0510开发板测量容量较大的电池,但输出的阻抗谱并不如小容量电池那样稳定,却没有规律。尝试对不同激励电压进行测试,阻抗图谱却没有发生明显的变化。

     测试结果如下:1.交流电压100mV+直流偏置电压100mV; 2.交流电压600mV+直流偏置电压100mV(交流>直流); 3.交流电压600mV+直流偏置电压1200mV(可设置的最大值); 4.交流电压300mV+直流偏置电压1200mV(软件默认值)。 四种情况下阻抗谱无明显区别,重合度高。

     需要对较大容量的电池进行测试时是否可以考虑增大电流呢? 用户手册说环路电流是50mA,那我能否通过降低62Ω电阻的方法来达到提升电流的目的呢?或者可以通过软件代码来设置?这点在数据手册并没有讲明,需要您指点一下。 谢谢!