成员
标签
Cancel
问答
Threads
97 Questions
Tags
RSS
More
Cancel
All recent questions
Unanswered questions
Answered questions
Questions with suggested answers
Questions with no replies
By title
By last reply date
By thread date
By reply count
By view count
By most asked
By votes
By quality
Descending
Ascending
by
dfdtc
能源存储系统(ESS)和电池管理系统(BMS)
Started
3 months ago
157
0
0
Not Answered
LT8708-1手册框图中显示IMON_ON实际感测正向Iout
0
Not Answered
LT8708中,Iout方向表述为From controller Vout, To system Vout,也即从CSPOUT->CSNOUT; LT8708-1手册表示Iout感测引脚仅有IMON_ON可用,其输出电压正比于负向Iout,具体使用方法参考LT8708的手册,然而其手册中的框图似乎显示IMON_ON输出为放大的(CSPOUT-CSNOUT),该数值在正向Iout才为正数
Datasheet/Specs
battery charger ic
LT8708-1
battery management
157
0
0
by
dfdtc
能源存储系统(ESS)和电池管理系统(BMS)
Started
3 months ago
357
0
0
Not Answered
Can LT8708 be used as follower in multiphase system?
0
Not Answered
I want to use LT8708s to build a multiphase DC-DC converter. I see that LT8708-1 is the product which can be operated as follower . But LT8708-1 have not such easy to buy in my country, most distributor not provide it, or it will be really expensive and...
hardware
battery charger ic
multiphases
External Power Switch Buck-Boost Controllers
LT8708
battery management
Buck-Boost Regulators
power
Show More
357
0
0
by
venu2105
能源存储系统(ESS)和电池管理系统(BMS)
Latest
3 months ago
by
ADIApproved
521
2
0
Answered
Cell balancing
0
Answered
Hello Team, I am currently working with the ADBMS6830 battery monitoring IC for a cell balancing application and would like to clarify some observations related to balancing behavior during ADC operations. In my design, I am using an external NMOS...
hardware
Battery Monitors & Fuel Gauges
battery management
ADBMS6830
521
2
0
by
MXY
能源存储系统(ESS)和电池管理系统(BMS)
Started
4 months ago
201
0
0
Not Answered
LT8491首次上电是否需要配置寄存器
0
Not Answered
请问一下,LT8491这颗芯片根据手册推荐电路搭建demo板,在首次上电时是否需要先配置寄存器相关参数呢?我做了两块样板,有一块是可以输出的,但是输出电压与设计值有一些偏离。如果采用出厂默认参数,能否进行正常的MPPT充电,请各位大佬解答一下。另外,如果配置寄存器比较麻烦,打算选型LT8490芯片,芯片工作时噪声如何,因为有测量充电电压、电流的需求,在绘制PCB时如何考虑ADC电路与芯片的布局关系呢。 PDF
hardware
battery charger ic
battery management
LT8491
201
0
0
by
LLLGYLLL
能源存储系统(ESS)和电池管理系统(BMS)
Latest
5 months ago
by
LLLGYLLL
478
2
1
Answered
ADBMS1818均衡问题
0
Answered
你好请问大家,带外部均衡电路ADBMS1818板子,上电后电池会烧毁采集电路上的100Ω电阻,尝试换10Ω电阻依然不行,电阻封装为0805,这是哪里的问题。
hardware
battery management
Multicell Battery Stack Monitor
ADBMS1818
478
2
1
by
ydp123
能源存储系统(ESS)和电池管理系统(BMS)
Latest
6 months ago
by
BMS123
1205
8
0
Suggested Answer
LTC6820+ADBMS1818架构下,EFT测试时菊花链通讯干扰问题,报PEC错误
0
Suggested Answer
ADI团队您们好。 我们在使用LTC6820+ADBMS1818组成的BMS系统做EFT测试(从AC端口L/N/PE分别注入组合波±2kV,频率5kHz)遇到菊花链受到干扰,报PEC错误的问题。 架构图如下:系统包括1个主控和8个从控,他们之间用双绞线束连接(非屏蔽线束);主控上放置LTC6820+通讯隔离变压器(74941300伍尔特); 从控上放置ADBMS1818+ 通讯隔离变压器(74942402 伍尔特)。 通讯链路的硬件配置参数分别如下: 请帮忙看一下...
hardware
1205
8
0
by
taoking
能源存储系统(ESS)和电池管理系统(BMS)
Started
7 months ago
213
0
0
Not Answered
接近满电的电池,放置一段时间后,mcu重新配置一次电量计配置参数,获取的soc为25%左右
0
Not Answered
我之前测试过,如果只在电量计掉电前配置一次电量计,在几次充放电后,满电后电量计的soc只有80%左右,为了不出现这个问题,每次系统上电时,都会重新配置一次电量计。总共几十台设备,出现了2台设备获取的soc为25%左右,插入适配器冲一会电后,电量会达到95%,mcu断电静置一段时间后重新配置一次电量计,soc又会变为25%左右
m5
software
ez
Battery Fuel Gauge and Coulomb Counter
电量计
max17261
battery management
Show More
213
0
0
by
taoking
能源存储系统(ESS)和电池管理系统(BMS)
Started
7 months ago
208
0
0
Not Answered
聚合物锂电池在多次充放电后,达到充电芯片的充电截止电流后,MAX17055获取的电量不是100%,只有83%左右
0
Not Answered
按照《max17055-software-implementation-guide.pdf》中描述的OPTION1配置 DesignCap 、 VEmpty 、 ModelCfg 、 IChgTerm ,开始的几次充满电后,MAX17055获取的电量可以达到100%,之后会出现达到充电芯片的充电截止电流并停止充电后,MAX17055获取的电量只有83%左右
software
Battery Fuel Gauge and Coulomb Counter
MAX17055
电量计
battery management
Show More
208
0
0
by
ydp123
能源存储系统(ESS)和电池管理系统(BMS)
Latest
7 months ago
by
ydp123
486
2
0
Answered
LTC6820设置为主机模式,引脚MISO波形异常
0
Answered
ADI团队您们好。 我们使用LTC6820+ADBMS1818调试遇到问题,LTC6820设置为主机,连接1片ADBMS1818。LTC6820的MISO引脚低电平时出现很高的电压尖峰(出现在时钟SCK的下降沿)。 核对LTC6820手册,也看到时序图中有同样的尖峰,如下是规格书中的时序图和实测波形图(紫色为SCK,蓝色为MISO)。 请问这个尖峰代表什么状态吗?是LTC6820发出的?有办法消除吗? 期待您们的答复。
hardware
486
2
0
by
wmq
能源存储系统(ESS)和电池管理系统(BMS)
Started
8 months ago
169
0
1
Not Answered
undefined
0
Not Answered
DS2788在给电芯建模时,放电倍率有什么要求吗?老化的时候,充电放电电流有限制吗,比如说不能超过多少A。充电放电之间的时间间隔多久比较合适呢? 电池一般在-40℃~60℃使用,电芯建模时,挑选哪五个温度建模会比较好?考虑到低温电池不能充电,如果需要在0℃以下的电芯建模,如何设置电芯的充放电环境温度会比较好一点?
Datasheet/Specs
DS2788
Battery Fuel Gauge and Coulomb Counter
battery management
169
0
1
by
china111
能源存储系统(ESS)和电池管理系统(BMS)
Started
8 months ago
162
0
0
Not Answered
电量
0
Not Answered
目前在使用这个ic的时候按建模好的参数的配置老化学习以后,发现一个问题电量不准的问题。 我用0.5A放到6.0V,然后0.6A充到8.2v,截至50mA
software
DS2776
Battery Fuel Gauge and Coulomb Counter
DS2776G+
battery management
Show More
162
0
0
by
china111
能源存储系统(ESS)和电池管理系统(BMS)
Started
8 months ago
110
0
0
Not Answered
密钥和电量问题
0
Not Answered
我在使用中客户要求写入密钥,规定了secret的密钥内容,我用上位机进入这个,write Challenge和Read ROM .33h, 手动写入secret,lock,Compute MAC,这样子显示,然后我通过上位机断开通信以后就发现,前面写的内容不见了。请问完整的密钥写入是如何。我的操作有什么问题,谢谢
software
DS2776
Battery Fuel Gauge and Coulomb Counter
DS2776G+
battery management
Show More
110
0
0
by
LTC4100
能源存储系统(ESS)和电池管理系统(BMS)
Latest
10 months ago
by
LTC4100
425
2
1
Not Answered
咨询LTC4100充电位恩特
0
Not Answered
想咨询一下LTC4100充电问题,目前按照LTC4100开发板电路参考设计,MCU这边可以通过SMBUS和芯片进行通讯,DCIN接12v,电池接上电压7.16V左右,CHGEN接到MCU,给了低电平,ACP 1.04V,软件读到charger_status:0X104C,可以帮忙看看是哪里的问题吗?
Switching Battery Chargers
software
battery charger ic
LTC4100
425
2
1
by
Chio
能源存储系统(ESS)和电池管理系统(BMS)
Latest
11 months ago
by
Chio
550
1
0
Not Answered
MAX17261 EZ模式评估电量时,放电到1%后会保持1%很久(几乎相当于30%电量时长),经过多轮充放电仍如此,为什么
0
Not Answered
采用MAX17261 EZ模式评估电量,放电到1%后会保持1%很久(几乎相当于30%电量时长),经过多轮充放电仍如此,为什么。 普通聚合物锂离子电池,2串,5Ah,3mohm采样电阻,2.5A充电,平均约400mA放电(有60Hz左右的工作节律),repcap指示约5000mAh,current和avcurrent基本都是400mA,满电放电8-9小时后就显示1%电量,但电池电压仍有3.6V,仍能持续放电约3小时才会到0%,为什么?
software
Battery Fuel Gauge and Coulomb Counter
max17261
battery management
550
1
0
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.