Article MAX6951CEE+輝度レジスタの解釈

Question:
RSETでピーク電流を40mAとして、輝度レジスタを15/16に設定した場合に37.5mAとはどういうことでしょうか。

200usの1/16の時間12.5us当たりは2.5mAしか流れず、200usの15/16の時間の合計が37.5mAということでしょうか?

それとも37.5mAの電流がある時間流れるのでしょうか?もしある時間流れるのであればその時間はどれくらいでしょうか?

 

Answer:

2.5mAと37.5mAなどは動作中に単位時間内の消費電流です。

仮に、LEDがONの時に流れる電流が一定になる、

ONの時間の長さによって、1サイクル当たりの動作電流は異なります。

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.