Article 为什么MAX17055在电池充满后测量到的电量达不到100%?

使用MAX17055可以不对电池进行建模就可以得到较精确的电量测量,只需要对MAX17055进行简单的配置,如果电池容量,充电截止电流,满电量电压。但是需要注意的是,所配置的电池容量与电池的实际容量相差不能太大,否则可能出现不能测量到满电量的情况。比如电池的实际容量是1000mAh, 将MAX17055中的电量寄存器配置为2000mAh,即使经过多次充放电,MAX17205也不能将电量修正到1000mAh。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.