MAX17262MEWL+: FAQ
文档
问答
Members
Tags
Cancel
文档
MAX1x
MAX17262MEWL+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
为什么MAX17262的内部检流电阻是7mohm,但是在计算电流或容量是却按10mohm计算?
MAX17262确实使用了一个高精度的7mohm内部检流电阻来测量充放电电流,但是在实际计算电流或容量的时候所使用的Resolution却使用10mohm检流电阻,这是因为MAX17262之前的几款电量计如MAX17055等都是使用外部检流电阻,而10mohm的外部检流电阻更通用一些,所以我们的评估板上使用的都是10mohm的检流电阻,计算容量,电流等参数时也是按10mohm来计算的,这样更方便一些…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.