MAX17261METD+: FAQ
文档
问答
Members
Tags
Cancel
文档
MAX1x
MAX17261METD+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX17261G应用在多节电池时会测量电池总电压吗?
MAX17261并不是测量电池的总电压,而是通过分压电阻测量单节电池电压,再根据寄存器中的电池节数去计算总的电池电压。
MAX17261如何使用软件POR复位?
MAX17261的软件复位命令如下: Data 0x59 written to address 0x62; Data 0xC4 written to address 0x63;//Unlock Model Access Data 0x00 written to address 0x80; Data 0x0F written to address 0x60;//POR command…
MAX17261数据手册中VEmpty寄存器的分辨率为10mV,初始值为0xA561,计算后得到的为1.65V,为默认值一半,请问该如何计算?
正确的计算为: initial Value: 0xA561 = 1010,0101,0110,0001 VE占据D15--D7共9位, 也就是 1010,0101,0 这个时候重新按照4位排列如下: 1, 0100,1010 =14A=330*10mV=3.3V
电量计在多串应用的考虑
Maxim的电量计产品已经发展到ModelGauge m5 EZ,支持免建模保证高精度,除了广泛用于手机、笔记本电脑等中低功率应用,也逐步向电动工具等高串数(>10S)/大电流(>20A)应用。 对于电动工具类应用,由于其使用时间/充电/放置时间的不确定,通常会对静态功耗提出很高要求,并希望在任何时候开机都立即得到比较准确的电量数据。目前客户一般会在空置时关闭主控板电源,而电量计部分则需要长期工作…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.