MAX17048: FAQ

  • Created
  • Updated
Was this helpful?
  • MAX17048的Crate寄存器含义及计算方法

    Crate 用来表示放电或充电的速率,它的 单位既可以是%/Hr,也可以是C。其中%/Hr表示每小时电量增加或减小的百分比;当用C表示充电或放电速率时,1C = 100%/Hr。例如,对于一个容量为1000mAh的电池,当放电电流为100mA时,可以说放电速率是10%/Hr,也可以说是0.1C. Crate的计算是将0x16寄存器的值转换成十进制,再乘以0.208%/Hr。需要注意的是,这个寄存器的最高位为符号位…
  • 数据手册没有描述MAX17048关断(shutdown)模式,可否提供具体说明?

    数据手册参数表后面的Note 6指出:The IC enters shutdown mode after SCL < V IL and SDA < V IL for longer than 2.5s. 但没有给出关断模式的具体说明。从这里描述的条件看,实际上指的是“休眠状态(sleep)”,此时IC关闭所有操作,电源电流降至1µA以内。休眠模式下,IC不对自放电进行检测。退出休眠模式后,进入常规操作

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.