MAX14690AEWX+: FAQ
文档
问答
Members
Tags
Cancel
文档
MAX1x
MAX14690AEWX+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX14690A当接入BAT的时候, SYS的电压并不是BAT的电压,而是0.75V左右,为什么?
在BAT处加上电池后,SYS处有一个1V左右的电压并且这个电压是在逐渐下降的。但是将电池接到SYS后,BAT处的电压比电池电压低0.3V左右,所以有可能MAX14690内部的连接SYS与BAT的MOSFET的漏-源极是和外面的P-MOSFET的漏-源极相反的。所以内部BAT与SYS并不能通过内部MOSFET的体二极管相连,必须要在MAX14690处于on mode时内部MOSFET才能导通。而外部P…
如何将MAX14690配置成on mode?
可以先读取PwrRstCfg寄存器的值,然后根据读到的值找到datasheet第18页图1 Power Function Input Control Modes Flow Diagrams中对应的流程图,并根据流程图中的指示来将MAX14690配置成on-mode。例如,PwrRstCfg寄存器的值为0110,则可以找到第18页的第四个流程图,也就是CUSTOM BUTTON MODE,然后将CHGIN…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.