DS2788E+: FAQ
文档
问答
Members
Tags
Cancel
文档
DS
DS2788E+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
8节磷酸铁锂电池电量计选型
8节磷酸铁锂电池电量计可以使用MAX17205,但是由于不同酸铁锂电池的特性相关较大,在使用MAX17205之前需要根据电池特性以及应用条件对电池进行建模,这样才能准确测量电池电量。
DS2788在单节电池应用中是否Vdd电压要大于Vin电压,才能准确测量电池电压?
DS2788的供电电压VDD要大于检测电池电压的引脚VIN处的电压才能准确测量电池电压。DS2788的datasheet第二页中规定VIN电压要在0至VDD之间,也就是VDD要大于VIN。
DS2788支持多个MCU读取数据吗?
DS2788采用单总线的通讯方式,如果处理器在不通讯时配置为漏极开路的方式,可以支持多个MCU读取数据,但在任何时刻,确保只有一个MCU和DS2788进行通讯,如果多个处理器同时向DS2788发送数据会造成数据错误,导致无法进行通讯。
DS2788数据手册给出了两个温度: "-25~70"(1st page) 和 "-40~85"(2nd page) ,区别是什么?
第1页给出的 "-25~70" 是典型工作温度; 第2页给出的温度"-40~85" 则是额定极限值。
DS2788是否支持多个MCU读取数据?
DS2788采用单总线的通讯方式,如果处理器和DS2788连接的引脚在空闲时配置为漏极开路的方式,可以支持多个MCU读取数据,但在任何时刻,确保只有一个MCU和DS2788进行通讯,如果多个处理器同时向DS2788发送数据会造成数据错误,导致无法进行通讯。
DS2788电量状态(SOC)显示不准确,为什么?
问题描述:我们有一个电路使用DS2788提供电池电量指示。已经根据我们的电池规格配置了EEPROM。我们设置为使用4颗LED表示充电状态。将电路连接到“耗尽”的电池时,1颗LED闪烁,随着电池充电LED点亮,然后当完全充满时4颗LED全部点亮。看起来工作正常。但是,如果将该芯片安装到另一块电路板,使用 已经充满 的电池,也是1颗LED闪烁,好像电池没有电似的。有没有办法使芯片在连接到不同电池时进行复位…
DS2788监控多于10个串联电池的使用情况时,通过调节分压电阻是否还适用?
从理论上来讲是没有问题的,无论多少节的电池,对于DS2788而言都是分压后做成1节电池进行测量的,但是在实际应用中有一个问题:找到一个高压的LDO稳压器来支持将输入电池电压转换成4.5V的DS2788供电电压,并且要求LDO的静态功耗非常低,因为,LDO本身消耗的电流DS2788无法计量。当LED点亮时, LDO消耗的功耗将非常大,也要考虑LDO本身的功率耗散,外部分压的MOSFET同样也要可以支持更高的电压…
DS2788芯片需要单独写程序?
DS2788是一款基于库仑计的电量计,该电量计主要应用在电池包内,或者说电池和电量计不分开的场合。在使用该电量计时需要根据具体的应用和使用电池的特性来配置内部的寄存器,因此,需要写程序来配置,也可以购买Maxim的评估板对内部的寄存器进行配置,内部的寄存器时非易失寄存器,因此当一次配置完成后,就可以独立工作,此时就不需要单独的程序来控制,DS2788可以驱动外部的5个LED来指示剩余电量。
使用DS2788设计的电量计,其外部LED一直亮着,为什么?
DS2788上电后PIOSC寄存器的第1位默认值为1,不需要配置这个寄存器,PIO引脚识别到上升沿后就会使能电量显示;如果往PIOSC中写入0,则PIO为开漏输出驱动,此时即使PIO引脚上有上升沿也不会显示电量,需要将PIOSC写入1后再给上升沿信号才能显示电量。正常情况下不会出现LED一直亮着的情况,因为LED点亮后不管PIO引脚状态如何,4秒后LED都会熄灭。LED一直点亮很可能是所使用的DS2788质量有问题…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.