DS2781G-A2+: FAQ
文档
问答
Members
Tags
Cancel
文档
DS
DS2781G-A2+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
DS2781G-A2+T&R与DS2781G+T&R的区别是什么?
DS2781G-A2+T&R中的A2代表特定的die版本,DS2781G-A2+T&R的价格与DS2781G+T&R不一样。对于普通应用请使用DS2781G+T&R。
在使用DS2781时单独给VDD供电引起的问题
如果单独给DS2781,当把电池拿走后,此时由于DS2781的供电还在,所以它仍然可以检测电池电压,由于电池电压突然变为0V(电池移除),DS2781检测到有效空电量,认为电池没电了,会把ACR清零,所以再把这个电池连接到DS2781后,即使电池有电,电量也会显示为0。而如果供电引脚VDD和电压检测引脚VIN同时连接到电池,当电池移除后,由于DS2781没有供电,所以它不能检测到有效空电量,ACR里的值可以保存到EEPROM里…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.