DS2781E+: FAQ
文档
问答
Members
Tags
Cancel
文档
DS
DS2781E+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
DS2781参数模型中线段斜率的计算公式中为什么要除以(1051mAh / 1M)?
((1031mAh – 1009mAh) / (1051mAh / 1M)) / (18ºC - 0ºC) = 1163ppm/ºC 这个公式可以理解为(1031mAh – 1009mAh) /(18ºC - 0ºC) 再除以(1051mAh / 1M),其中(1031mAh – 1009mAh) /(18ºC - 0ºC)得到的值类似于斜率,但是它的单位是mAh/ºC,将这个值再除以(1051mAh…
在使用单片机读取DS2781内部的数据时,如果需要读取不连续的两个地址,该如何操作?
有两种方法可以实现读取非连续地址的数据: 1. 利用一个读取命令连续读取多个字节,然后只处理需要的两个地址的字节。 2.单独读取,这样每次读取都需要发送复位命令,ROM命令然后再读取相应的寄存器。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.