DS2780在电池没有充放电的情况下读到有较大电流(2-10mA)流过检流电阻,原因是什么?
文档
问答
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
over 2 years ago
文档
DS
DS2780E+: FAQ
DS2780在电池没有充放电的情况下读到有较大电流(2-10mA)流过检流电阻,原因是什么?
由于VDD与VSS之间的0.1uF电容离DS2780较远,而给DS2780供电的MAX1616的输出电压纹波较大,导致有干扰进入到DS2780。加大MAX1616的输出电容,并在靠近DS2780的VDD和VSS处加一个0.1uF的电容后,在没有充放电的情况下,DS2780检测到的电流在0.1mA以下。
DS2780
000096486
能源存储系统(ESS)和电池管理系统(BMS)
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.