DS2780E+: FAQ
文档
问答
Members
Tags
Cancel
文档
DS
DS2780E+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
DS2780在电池没有充放电的情况下读到有较大电流(2-10mA)流过检流电阻,原因是什么?
由于VDD与VSS之间的0.1uF电容离DS2780较远,而给DS2780供电的MAX1616的输出电压纹波较大,导致有干扰进入到DS2780。加大MAX1616的输出电容,并在靠近DS2780的VDD和VSS处加一个0.1uF的电容后,在没有充放电的情况下,DS2780检测到的电流在0.1mA以下。
可以正常获取DS2780的电压,电流等寄存器的值,且是正确的,但是关于电量的寄存器,如ACR,RAAC,RARC的值全是0,不知道是不是配置寄存器配置的不对,或者是什么其他的原因?
DS2780库仑计电量计要和电池一起使用才能够预报电量,通常使用时将电量计安装在电池包内, 这样在电池充电和放电时电池和电量计都在一起,可以计量流入和流出电池的电量,除此之外,还有一些内部的寄存器需要设置,您可以参考下面的文章来理解库仑计电量计的使用 http://blog.sina.com.cn/s/blog_a0a27b830102wdcw.html
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.