DS2745U+: FAQ

  • Created
Was this helpful?
  • DS2745测量电量误差是多大?

    根据数据手册: Current Offset IO ERR (Note 2) -7.82 +12.5 V/R Current Resolution ILSB 1.56 V/R 芯片的active current 为70uA 电流增益误差 Current Gain Error 为-%1 to +%1 检流电阻不一样会影响offset 和 分辨率。假设检流电阻为20mOhm。 假设目前实际值为1mA,…
  • DS2745自身电流损耗怎么考虑?

    DS2745 在 工作状态active current 为70uA,待机状态Sleep-Mode Current静态电流为1uA。 这部分电流不流过检流电阻。因此读数不包含这部分电流。但DS2745工作电流和静态电流很低,相对于实际外部电路的电流,可以忽略不计。因此对测量电量的精度是关键因素。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.