问题描述:
以前利用MAX11410来实现两通道测量,采用AIN0作为恒流源, AIN1和AIN2作为测量通道,实际应用中测量的温度精度符合要求,在新设计中需要实现4通道的测温,为节约通道采用了AIN0既作为恒流源,有作为测量输入通道,发现测温误差很大,请问这样设计是否有问题?
------------------------------------------------------------------------------------------------------------
问题答复:
由于内部的各个通道具有多种配置,内部采用了模拟开关进行功能切换,模拟开关的导通电阻导致了这个测温误差,因此,在设计时不能把一个通道同时配置为既做为恒流源,又作为测量输入,这样恒流源流过内部的模拟开关后会造成测温的误差,一定要按照数据手册的推荐电路来进行设计,如果需要实现4通道的设计,可以通过外部增加模拟开关的方式来实现,Maxim可以提供这样的参考设计--MAXREFDES1154.