您好,想利用QuartusII软件,利用FPGA读写ADT7410芯片。因此我的思路是首先对芯片内部相关寄存器进行配置,如地址为0x03的配置寄存器(configuration register),配置为8'b10000001(默认是8'b00000000),因此按照datasheet中的时序图进行编程配置。但是波形的输出中ack始终无应答。如图所示,ccs(第三行的信号)可以当做scl的计数信号,当ccs=0时,让FPGA控制sda在scl为高电平时产生下降沿,作为开始信号。接下来写入10010000(7位从机地址和一个R/W位),然后在ccs=9时我让FPGA将sda拉高。我的理解是此时ADT7410会使sda从高变为低作为ack位,但波形中并没有ack位。
另外,下个图作为参考,从ccs=10开始,希望写入配置寄存器的地址0x03(8'b00000011),这样第18位应该也产生一个ack位,而实际并没有。
不知道问题出在哪里。硬件连接无误,scl我设置的是200kHz的频率,scl为output,sda为inout.谢谢!