Post Go back to editing

关于AD7763内部增益寄存器问题

AD7763 datasheet中对于内部增益寄存器介绍的不够详细,只是说明了默认值为1.25,我想问下内部增益寄存器的值是否可以改变?如果可以改变那么改变的范围是多少,或者这个改变值和谁相关?

我的压力传感器的灵敏度为2mv/v,激励电压为5V 最大可以输出10mv, 输入AD7763的模拟信号范围为0.05mv~10mv,由于PCB空间限制所以不准备用外围放大电路,准备直接用AD7763内部差分放大器和调节内部增益进行信号放大,不知道我的想法是否正确,请大家帮忙~谢谢