Post Go back to editing

AD9042S的数字供电为5V,能不能与3.3V的FPGA直接相连?

AD9042的数字供电是5V,但是FPGA只有3.3V的IO,可以直连吗?如果不能可有什么解决方案

  • 不建议直接连接使用。建议使用电平转换芯片进行处理,如ADI的ADG3300系列,或者其他厂家,如TI的SN74L系列电平转换器件。对于AD9042其实也可以考虑使用串联电阻的方式进行处理,但是要考虑因为电阻和分布电容带来的滤波效应,以免影响数字信号的正常传输。