ADR3412输出电压波动

使用ADR3412产生1.2V参考电压,3.3V供电,测量输出只有1.194V,达不到0.1%的初始精度,请问有可能是什么原因造成的?

另外,电路中有一个5V供电的433MHz无线模块,当模块工作时,ADR3412输出电压会发生较大波动,变化范围可以达到0.04V,完全不能使用,请问造成这种情况的原因有哪些?

Parents Reply Children
No Data