Post Go back to editing

AD5676R的问题

现在是这样的,下面是原理图(基本采用EVAL-AD5676SDZ_5676RSDZ_UG-814.pdf)

现在的问题是我在调试的时候发现Vout电压上不去,我这边给的VDD和Vlogic是3.3V,Vref电压2.5V,GAIN也是拉到Vlogic,应该来说我这个电路输出的幅度在0~5V之间,现在我调试的时候 ,把输出的幅度调整到5V,但测下来发现最高只有3.3V,3.3以下的电压都是正常的,固件这边,数字量给一半的数据也能显示2.5V,给满量程的数据就只有3.3V,能看看怎么回事吗?

  • 您好,感谢对ADI的关注。

    AD5676R的输出级放大器是轨到轨的运放,其输出电压范围是0V到VDD。您使用的是3.3V供电,所以输出会钳位在3.3V。

    The output buffer amplifier generates rail-to-rail voltages on its output, which gives an output range of 0 V to VDD.

    您可以尝试把VDD接5V,输出应该就能达到0-5V范围了。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.