Post Go back to editing

AD7357芯片CS一直拉低无法输出采集数据?

实验中使用AD7357芯片,采集100KHz的正弦信号,通过SPI方式获得采样数据,SPI的sclk为2.8MHz;

     1.   在我实验过程中,如果将CS拉低,再使能SPI,然后SPI为AD7357提供2.8MHz的sclk,按照理论上,ad7357有SDATAA和SDATAB共32位二进制数据输出,但是AD芯片没有数据输出?

     2.   实验又采用CS拉低使能SPI,然后运行32个时钟周期,关闭SPI,并将SPI拉高;然后循环这个过程才能产生数据。

问题:请问是不是只能将CS循环置0和置1执行16或者32个周期才能输出数据呢,如何实现CS拉低,使能SPI后,一直产生数据呢?

     谢谢

Parents Reply Children
No Data