Post Go back to editing

AD2S1210 寄存器读取

工程师你好,我在配置模式下写入和读取配置寄存器时发现一些奇怪的现象,寄存器地址为偶数的时候,内容只能写进去一次,再次读取的时候内容就变成了0,地址是奇数的时候,则没有这样的问题,读写都正常。比如,DOS失配阈值寄存器,我第一次写入数据以后,DOS超过失配阈值故障不会报错,当我读取这个寄存器的时候,读出的内容是0,同时DOS故障灯亮,读取一次错误寄存器(奇数地址)显示是0,灯灭(读取其他奇数寄存器,显示正常,灯也会灭)。还有一种情况是,第一写入DOS失配阈值寄存器没有错误,读取内容之后为0,DOS故障灯亮,再读错误寄存器,灯不会灭,同时错误指示为DOS超过失配阈值故障。这些现象如何解释?还有一个问题是,使用AD2S1210读取位置和速度各一次的时间多少算正常?我用的28335,主频150M只读位置和速度用了大概30us。