大家好:在使用AD7357时,单通道输出不准确和采样频率提高后数据采样不准确

大家好,我在使用AD7357时候,参照的推荐电路AD8138+OP177+AD7357的电路,采集10k~1MHz信号,遇到以下问题:环境(STM32F429+AD+SPI+DMA)

1. 这款AD7357芯片能够使用SPI的方式传输采集的数据吗?

1. 使用标准正弦信号通入SDATA_A中,输出采样数据为,这个波形的差分信号波形。意思也是,只有将采集的相邻两个数据分开然后形成两组数据,最后绘制为一对差分正弦信号;正确的应该是一个标准的正弦波吧?

2.在两个通道的输入都为100K正弦信号,在SDATA_B通道输出两路信号采集数据。当使用DMA+SPI的通信速度为1.4MHz采集数据时,能够输出正常数据,但是当SPI的通信速度为2.8MHz时,数据就完全不正确了,但是数据范围正确的0~16383,请问什么原因导致的呢