AD7173-8的输出问题

在调试AD7173-8的时候,首先发送了读IP寄存器的命令,收到的回复是30D5,也即SPI通信无误。然后将CS拉低,DIN保持高电平,但是一直等不到DOUT为低电平的状态。看datasheet上说明,默认为连续转换模式,在一次数据转换完成后在CS为低电平时DOUT变为低电平,然后可以发送命令0x44读取数据,但是我都没见到DOUT有低电平的时候,请问各位专家如何解决?

我如何不管DOUT是否为低,直接发送0x44命令,读到的数据是个固定值。