Post Go back to editing

32位ADC芯片的前端设置问题

在寻求一款32位ADC芯片,需要的采样频率在4kHz~16kHz,ADC输出频率1kHZ,有效分辨率至少20位。

希望ADC前端的低通滤波把系统带宽限制在840Hz。查询到LTC2508-32,LTC2500-32以及AD7177-2三款产品,

想了解如下情况:

       1、不知道还有没有可推荐的32位ADC?

       2、我的信号是单端输入,应该需要一个单端转差分的运放,希望该放大器有可配置低通滤波器,这样可以简单地设置

低通滤波截止频率在840Hz,能否推荐一些满足要求的放大器?

Parents Reply Children
No Data