Post Go back to editing

AD测量0-5V电压信号

如题,使用AD7782测量传感器输出的0-5V电压,应该如何搭建硬件电路呢?有几个问题请教大家,

1:根据手册,测量端Absolute AIN Voltage Limits范围是(GND+100MV,VDD-100MV),是不是意味着输入的两个引脚都必须是相对与AD的地有100mV的偏差呢,比如被测引脚A应该是0.1V-4.9V,被测引脚B也是,但是实际中被测引脚A就是地,被测引脚B会有0-5V变化,应用时是需要将被测信号抬升100mV吗?

2:由于后端接3.3V单片机MSP430,5V的AD和3.3V的430之间如何连接呢,是否需要电压转换?