按照芯片手册,AD7902的功耗最大只有12mW,而ADP7104的接地电流也很小,但是在使用工程中发现ADP7104与AD7902组合时,ADP7104的工作电流达到了75mA左右,有时甚至能超过100mA。电路我是参考了AD7902评估板的电路。具体如下:
这部分我使用7.5V供电。
7104我买的也是2.5V固定版本
R6,R8,R9其实并没有特别的用途,实际使用中如果连接R6,那我就是用3.3V对7104供电,R9如果连接就是使用7.5V供电,R8一开始打算分压用的,但是实际上并没有连接过
7104我买的也是2.5V固定版本
R6,R8,R9其实并没有特别的用途,实际使用中如果连接R6,那我就是用3.3V对7104供电,R9如果连接就是使用7.5V供电,R8一开始打算分压用的,但是实际上并没有连接过