如何保证2片AD9735的同步

我的设计中使用2片DAC(AD9735)产生I和Q基带信号,同时,AD4350产生2.4GHz本振。然后通过正交调制(选用ADL5385),产生载频为1.2GHz的调制信号。2片DAC时钟由AD9516提供600MHz时钟。FPGA为2路DAC输出IQ数据,该数据保存在一片ROM中,从而保证IQ基带信号的严格对起。现在发现,2片AD9735的输出发生错位,错位0~4个DAC时钟周期。而且,每次上电后,错位情况都不一样。但是,上电后,错位保持不变。DAC的配置:每次上电后,同时对AD9735进行硬件复位(使用同一个复位信号),其他都是默认配置。IQ的信号是75MHz信号,ADL5385的本振信号是2.4GHz。