Post Go back to editing

AD7799读取寄存器会出错

在读取AD7799寄存器的时候,有时候在读取STATUS REGISTER 时,会返回err。下图是AD的通道2的接入方式,

出现err的概率约为1/8,并无规律。

REFP接电阻到3.3V,REFN直接接SGND,

如果R40的另外一段悬空,则出来的ad值是2101,很稳定,也不会出现err,或者在R40端给一个小于10V的电平。也不会出现err,但是我在接上一个传感器后,传感器在正确环境下是0V的,AD值有从0跳到5000不等的变化,偶尔就出现读取寄存器错误,但是从示波器上看不到R40下端有输出超过10V的电压。不是很明白这个情况了~~求帮助