Post Go back to editing

AD8283时钟受HSC-ADC-EVALCZ干扰导致数据错乱!求助!

大家好,我近期正在使用AD8283这款芯片,配合着使用了专门的ADC数据采集板HSC-ADC-EVALCZ。

(图中是AD8283板与HSC-ADC-EVALCZ板的整体情况)

这两天新做了一块AD8283的板子和HSC-ADC-EVALCZ板一起配合采集数据,发现当AD8283的六个通道全部开启时,CLK+和CLK-信号受到了干扰而发生了畸变,导致VisualAnalog采集的数据不正常。

(上图是未受到干扰时AD8283的时钟情况(50MHz))

这个干扰通路目前看来是这样,AD8283的DSYNC和D0-D11上有快速跳变的高低电平(同步信号和转换数据),这些引脚接到了HSC-ADC-EVALCZ上,同时AD8283的CLK+和CLK-信号也接到了HSC-ADC-EVALCZ上,因此DSYNC和D0-D11信号变化引起的干扰就影响到了CLK+和CLK-,导致畸变,使得数据采集也不正常起来。

(上图是受到干扰后AD8283的CLK+和CLK-的情况)

按理说DSYNC、D0-D11、CLK+、CLK-对HSC-ADC-EVALCZ板来说都是输入信号,彼此之间不应该有干扰的,所以目前的这种现象让我很困惑,不知道原因,也不知道该如何解决。

(上图是受到干扰后AD8283采集的数据在VisuaAnalog中的显示情况)

论坛里的大神们有没有遇到过类似的情况,有没有相关经验,可不可以帮忙分析下原因

很急,在线等!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.