Post Go back to editing

关于AD9212芯片的问题

关于AD9212芯片有以下问题,请解答!

1、AD9212的CLK+和CLK-可以直接由FPGA以LVDS信号提供吗(即FPGA输出引脚通过0.1uF电容直接连接到AD9212的CLK+/-引脚)?

2、AD9212 datasheet  Rev.E 中第22页Figure49单端信号输入图中的R、C、CDIFF的值分别是多少?实际应用电路可以按照该图直接连接2V的单端信号吗?

3、DRGND和AGND可以是一个地吗?在画PCB时需要分开模拟地和数字地,然后再单点将这两个地共地?还是没必要分数字地和模拟地,直接一个地即可?

Parents Reply Children
No Data