Post Go back to editing

AD5290模拟端无响应

     在连续使用AD5290芯片一个多月(期间芯片一直在工作)后,发现芯片的数字端通信正常,但模拟端突然失去任何的响应,我采用的是在VDD/VSS两端加+-12V的差分连接方式(对应的应该是datasheet上的divider连接模式),且A、B端输入电压要小于VDD/VSS(如果输入电压在额定范围内对应的A/B,A/W和B/W中的电流应该是小于5mA的吧),那么排除了过压或者过流损坏芯片的影响,我看了datasheet之后,对上电顺序和断电顺序还有静电防护都有一定的要求,我所有端口的上电顺序和断电顺序基本上是同步的,为了避免芯片能更好地持续工作,避免损坏。我想知道数字端能通讯模拟端无响应的这种情形是RDAC电路损坏了吗?如果是这种情况,有可能是什么原因?芯片损坏的原因除了VDD/VSS、A/B输入端电压和A、B、W间电流要控制,还可能是什么原因?很急,希望得到快速的回复,谢谢。