Post Go back to editing

AD7091-R8

目前用AD7091-R8设计一款8路电压采集模块,AD7091的模拟输入范围是0~Vref(2.5V)。

需要采集的目标电压是0~10V,计划使用运放ADA4807(替换ad8032)在前端设计电压跟随器。

在运放的正极使用分压电阻,使正极的输入把输入分压到0~2.5V,运放负极接输出,形成电压跟随器。

由于运放的输入阻抗是45兆欧,分压电阻是否取K级即可?

如果不想使用电阻分压的方法来调节运放正极的电压,前端是否有可选的芯片完成增益(0.2)调节功能(AD8475是否适用)?

是否有比AD7091-R8更为适合的ADC?(采样精度要求12bits,每通道采样速率250KsPs)