AD9287低温采样噪声问题?请帮忙

hi ADI专家,

signal chian: analog input-<AFE-<AD8334-<AD9287-100-<Xilinx FPGA.

Clock input:epson100M crystal oscillator from TI CDCV304 clock buffer.

1.8V analog and digital power all from TI TPS5430, analog and digital are from one supply connect bead between them.

问题条件描述:

1.产品在低温-10℃储存的情况下一小时(此时产品不上电),开机后,ADC采样波形底噪和毛刺明显,异常。大约8-10分钟热机后,异常消除。

2. 检查Clock和电源情况在异常的情况下并没有异常,AFE并无输入,也没有异常。

分析:

1.考虑到ADC和FPGA的功耗并不低(在常温板子有明显的热量),是不是在低温热机一会儿就正常,芯片低温问题?更换芯片后,有些可以好,有些还是不行。

2. 修改PIN40 电阻?10K 到1K,异常消除,此时IC功耗增大,手册中并没有对此说明,是否可以调整?是什么原因异常可以调整消除。

请分析下异常发生的原因,多谢!