Post Go back to editing

有关AD1871的评估板EVAL-AD1871EBZ的问题

新手求助:最近在做一个有关先天性心脏病心音采集的课题,因为需要用到低频部分的信号,所以需要用到AD1871。目前模拟的音频传感器是一般的电脑mic接口,想直接一点使用官方的EVAL-AD1871EBZ这个评估板,所以在这之前想评估一下这个板子是否可以使用,但是ADI网站上没有这个评估板的具体技术文档,只有AD1871的。各位大大或者官方的工程师能给我提供一下这个技术文档或者给解答一下接口方面的问题,是否有mic接口,是否存在单mic接口转双声道输入的问题,是否可以用STM32或者PC的USB端进行配置或者驱动,转换后的I2S信号是通过什么接口出来,是否可以通过USB接口传输到PC上或者通过STM32的I2S接口收集?

Parents Reply Children
No Data