Post Go back to editing

数模芯片AD5383使用中遇到的问题

ADI工程师:

    您好!最近购买了你们数模芯片AD5383和其他别的芯片(共计几千元,用于新项目的研发中),在使用AD5383中,数据无法更新,发现LOAD引脚上电就是高电平,那我还怎么把它置低写入数据呢,我使用的是SPI通信,目前卡在这个地方了,数据无法加载到输出引脚,很是苦恼,还希望你们能够提供技术支持 ,谢谢了!

    可以读芯片寄存器中的数据(已实现)!

  • //IO操作函数 

    #define SPI_SYNC    PEout(0) //SYNC

    #define SPI_SCLK  PEout(1) //SCLK

    #define SPI_DIN  PEout(2) //DIN

    #define SPI_SDA   PEin(3)  //输入SDA

    #define SPI_LDAC   PFout(0)  //LDAC

    AD5383程序如下:

    /********************************************************************************
    Function that writes to the AD5380 via the SPI port.
    ********************************************************************************/


    void WriteToAD5380ViaSpi(int32_t RegisterData)
    {

    long int ValueToWrite = RegisterData;
    int i;

    // SPI start

    SPI_SYNC=1;
    delay_us(1);
    SPI_SYNC=0;  //bring SYNC low
    delay_us(1);

    //Write out the ControlWord

    for(i=0; i<24; i++)
    {
      SPI_SCLK=1;
      delay_us(1);
      if(0x800000 == (ValueToWrite & 0x800000))
      {
       SPI_DIN=1;   //Send one to DIN pin
      }
      else
      {
       SPI_DIN=0;   //Send zero to DIN pin
      }
      delay_us(1);
      SPI_SCLK=0;
      delay_us(1);
      ValueToWrite <<= 1; //Rotate data
      delay_us(1);

    }
     

        // SPI ends


    SPI_SYNC=1;
       delay_us(5);

    }


    /********************************************************************************
    Function that read from the AD5380 via the SPI port.
    ********************************************************************************/


    void ReadFromAD5380ViaSpi(int32_t *RegisterData)
    {


    unsigned int     i = 0;
    unsigned int   iTemp = 0;
    unsigned long   RotateData = 0;

    unsigned long   Noop = NOP;

    // SPI start

    SPI_SYNC=1;
    delay_us(1);
    SPI_SYNC=0;  //bring SYNC low
    delay_us(1);

    for(i=0; i<24; i++)
    {
      SPI_SCLK=1;
      delay_us(1);
    //////////////////////////////////////////////////
    if(0x800000 == (Noop & 0x800000))
      {
       SPI_DIN=1;   //Send one to SDI pin
      }
      else
      {
       SPI_DIN=0;   //Send zero to SDI pin
      }
    //////////////////////////////////////////////////

      SPI_SCLK=0;
      delay_us(1);
       
      iTemp = SPI_SDA;   //Read DIN of AD5383, PE3
      RotateData <<= 1;
     
      if(iTemp==0X01 )
      {

       RotateData |= 1;
      
      }
     
      Noop <<= 1;
          delay_us(5);
    }

     
          
        // SPI ends

    SPI_SYNC=1;

        delay_us(2);
    *RegisterData=RotateData;

    }


    void ComPortsToPC(int32_t buf)
    {
    unsigned char tx[3] = {0,0,0};
      u8 t;
        tx[2] = ((buf)&0xFF0000)>>16;
        tx[1] = ((buf)&0x00FF00)>>8;
        tx[0] = (buf)&0x000000FF;
       for(t=0;t<3;t++)
       {
        USART_SendData(USART1, tx[t]);         //向串口1发送数据
        while(USART_GetFlagStatus(USART1,USART_FLAG_TC)!=SET);//等待发送结束
       }
      
     
    }

    主程序如下:

    main()

    {

    AD5383_Init();

    SPI_LDAC=1;

    delay_us(1);

    //-------------------------------------------------------------------------------------

    //Enable monitor and internal REF to 1.25v and select power down mode that is 100k_GND

    //-------------------------------------------------------------------------------------

    cstr = Write | Special_Function_Register | Control_Register  |Internal_REF_Enabled | Internal_REF_1_25 | PowerDown_100K_toGND| toggle_0_7;

    WriteToAD5380ViaSpi(cstr);

    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout0   |0x000FFF;  //Vout3 IS 0.6V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout1   | 0x000FFF;  //Vout3 IS 0.6V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout2   | 0x000FFF;  //Vout3 IS 0.6V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

      cstr = Write | Input_Data_Register | Channel_Vout3   | 0x000FFF;  //Vout3 IS 0.6V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout4   | 0x002000;  //Vout3 IS 1.2V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout5   | 0x000FFF;  //Vout3 IS 1.2V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout6   | 0x003FFF;  //Vout3 IS 2.4V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);

    cstr = Write | Input_Data_Register | Channel_Vout7   | 0x000FFF;  //Vout3 IS 2.4V
    WriteToAD5380ViaSpi(cstr);
    delay_us(1);


    SPI_LDAC=0;
      delay_us(1);
    //delay(2);
    SPI_LDAC=1;
    delay_us(1);
    //delay(2);

    while(1)

    {

      LED0=!LED0;   //闪烁LED,提示系统正在运行.

      LED1=!LED1;   //闪烁LED,提示系统正在运行.

      delay_ms(500);

    cstr = Read | Special_Function_Register | Control_Register; // readback control register data

       WriteToAD5380ViaSpi(cstr);                    

       ReadFromAD5380ViaSpi(&buf);   //Read select register, using two instruction cycles

      ComPortsToPC(buf);

    }

    }

  • 谁能帮帮我,谢谢了!

    #define SPI_SYNC    PEout(0) //SYNC

    #define SPI_SCLK  PEout(1) //SCLK

    #define SPI_DIN  PEout(2) //DIN

    #define SPI_SDA   PEin(3)  //输入SDA

    #define SPI_LDAC   PFout(0)  //LDAC

    STM32使用以上5个pin和AD5383进行通信,LDAC负责所有数据写完,拉低是数据加载到芯片输出引脚,是怪的是拉低此引脚时,低电平为0.93V,不能完全拉低啊???

    ADI的大神们,帮帮忙啊!

  • 在芯片上电后,LADA引脚为高电平,3.3V左右;STM32控制LADA的引脚不接芯片上,可以置低,为0V;接在芯片上后,低电平就是0.93V了;不能把LADA引脚拉置低电平;直接把LADA引脚接地,发现供电电源电流明显变大(增大10mA),感觉LADA引脚的高电平像是电源啊!

  • 还有这段代码对吗,写完8个通道的数据后,用下面的程序来加载数据,对吗?还是要写一个端口数据,加载一次?

    SPI_LDAC=0;

      delay_us(1);

    //delay(2);

    SPI_LDAC=1;

    delay_us(1);

    //delay(2);

  • 发一下电路吧, 仅仅只是凭叙述无法判断是什么问题

    因为 数字的输入电流只需要1uA足够了, 所以问题不应该出在驱动能力上

    是否有其他电路与此引脚连接,,导致电压无法下降

    此外LDAC的MCU控制引脚, 是否可以拉到地。。

  • Hi,all!

           十一加班调试板子,还好板子已调通了,不过这次我换成了IIC通信,就好了;不知道为什么SPI通信不可以,估计还是时序有问题吧!哪位大侠以后把SPI通信的程序调通了,还麻烦分享下,谢谢了!

           另外一点想提的就是为什么ADI的工程师那么不给力呢,出现的问题都没提供技术支持,如果产品研发成功了,最终受益的还是ADI公司啊,奇怪!!!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.