Post Go back to editing

AD9777输出频谱问题

我将35MHz采样率10MHz带宽的复基带信号用35MHz时钟分I、Q两路送进AD9777中,AD9777内设置内插倍数为8倍,Fs/4的IQ调制,complex mix mode,PLL ON,coarse gain adjustment设为最大值,fine gain adjustment设为零,offset adjustment设为零。

我从FPGA内送35MHz的时钟给AD9777做时钟,然后用AD9777返回的时钟来送基带数据。

在PCB板上对IoutA和IoutB进行差分转单端,用频谱仪观察输出的频谱如下图所示:

图中70MHz处带宽10MHz的信号是我想调制得到的中频信号,210MHz处的信号是-70MHz处经过280MHz采样率搬移的信号,这两个信号是我能理论解释的现象,但是在105、140、175、280MHz处出现的单音信号我却无法解释原因。希望高手帮我看看是什么原因造成的!

虽然这些单音信号能用滤波器滤除,但是,我想得到的信号70MHz处功率太低了。

我尝试基带送全零的信号给AD9777,用频谱仪测试得到的频谱仍然有那些单音信号,如下图所示:

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.