Post Go back to editing

AD5390输出为0无法正常输出,Reset后正常

我正在使用AD5390,通过SPI驱动,驱动时会首先Init芯片(一般只在上电时做一次),然后设置电压输出。有一次同事在测试中突然发现输出电压不对,用万用表测量发现其中2块板子的所有通道输出为0,但是芯片的SFR和x1寄存器的返回值和我设置的都完全一致,输出却始终为0。最后通过断电再上电,芯片输出才正常。后来我连接了12块板子,连续测试了40多个小时,输出都是正常的,这说明我的驱动和板子稳定性是没有问题的。我现在怀疑是芯片偶然进入了Power-Down状态,但是我没法读出芯片到底处在什么状态。因为我的应用是隔几秒改变一次电压值,那我是否可以每次都发一个Soft Power-Up防止芯片进入Power-Down?由于芯片已经处于Power-Up状态,再发Soft Power-Up是否对芯片没有任何影响?

1

attachments.zip
Parents Reply Children
No Data