Post Go back to editing

AD9755有如下两个疑问请帮忙解答

你好:

       我最近使用 AD9755有如下两个疑问请帮忙解答:

 

     1.  请问AD9755手册第16页,说使用变压器时中心抽头要接地(The center tap on the primary side of the transformer must be connected to ACOM ),这样DA的输出不就没有直流偏置了吗,会有负电压加到DA的输出端,而手册第5页又说这个管脚(IOUTA, IOUTB ACOM   –1.0 AVDD + 0.3 V)最大能承受-1V电压,是不是这个中心抽头不能接地啊?

 

    2.还是16页说使用11的变压器时使用50欧电阻接地,使用21时是75欧电阻接地功率从0dBm变到2dBm,不知道是怎么算的啊,还有我要使用3141的变压器是电阻应该是多少,输出功率又该是多少呢?

 

    请回复,谢谢,祝工作愉快。

Parents Reply Children
No Data