Post Go back to editing

AD7920不工作

我用AD7920进行AD变换,给定电源电压为5V,使用FPGAAD进行SPI通信,下面是电路原理图

但是实际测试中,给定模拟输出电压为2.5V(事实上无论给定电压是多少结果都一样)AD的输出一直是零。下面是FPGA输出的片选CS信号,和时钟信号,时钟信号频率为97KHz,采样频率为500Hz

1 片选信号与时钟信号,3个周期


2 片选信号与时钟信号,1个周期

1 片选信号与输出信号,3个周期

1 片选信号与输出信号,1个周期