Post Go back to editing

AD5260 在5v下工作正常,在12v下工作不正常

我搭了个数字电位器电路,期望使用Ad5260 数字电位器输出0v到12v的电压,我控制用的MCU的 gpio端口电压是3.3v的,vdd和A端输入电压为12v时不工作,改为5v时工作正常,难道SPI通信端口也要用12v电平?

Parents
  • AD5260的逻辑电源VL可以在2.7V到5.5V之间工作,且逻辑电平要满足如下要求,因此VL在3.3V供电应该是能正常工作的,另外VDD和VSS可以采用单电源12V供电,建议检查一下芯片AD5260的各个电源、数字控制口及输入输出的电平是否满足数据手册规定的范围,输入、输出电压都必须限制在VDD和VSS的范围,且MCU的逻辑输出的电平要满足如下的高低电平值,如果检查过都没有问题,建议你到我们的官网申请样片再测试一下。在测试的情况下,最好断开与AD5260不相关的器件进行测量。

Reply
  • AD5260的逻辑电源VL可以在2.7V到5.5V之间工作,且逻辑电平要满足如下要求,因此VL在3.3V供电应该是能正常工作的,另外VDD和VSS可以采用单电源12V供电,建议检查一下芯片AD5260的各个电源、数字控制口及输入输出的电平是否满足数据手册规定的范围,输入、输出电压都必须限制在VDD和VSS的范围,且MCU的逻辑输出的电平要满足如下的高低电平值,如果检查过都没有问题,建议你到我们的官网申请样片再测试一下。在测试的情况下,最好断开与AD5260不相关的器件进行测量。

Children
No Data